2018-02-22 1:11 AM
Hallo everyone,
I am working with the hardware kit �P-Nucleo-Azure 1� (STM32 Nucleo Pack for IoT node with Wi-Fi, sensors and NFC Connected to Azure cloud) and am having troubles in making it work.
I have imported the available Kile Project into Visual Studio with VisualGDB. Project is build successfully, but apparently the program does not recognize the correct motion board. In the �static void Init_MEM1_Sensors(void)� function, a macro is defined to choose the correct board (�&sharpifndef IKS01A2�), but this macro seems to not be used anywhere else in the program. Therefore, the program seems to not be able to choose the correct MEMS board.
Has anyone already had this issue?
I am using:
Thanks for any help!
William
#nucleo-l476rg #x-nucleo-iks01a2