cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble, need urgent help.

sima2
Associate III
Posted on February 10, 2011 at 16:10

Trouble, need urgent help.

10 REPLIES 10
ColdWeather
Senior
Posted on May 17, 2011 at 14:24

1. Have you enabled a clock to the timer anywhere like

RCC_APB1PeriphClockCmd (RCC_APB1Periph_TIM6, ENABLE);

2. Have you named an IRQ handler right?

void TIM6_IRQHandler(void)

 

{

 

...

 

}

3. Have you added the correct startup file to the project?

For instance, ''startup_stm32f10x_hd.s''. Look inside your startup file: can you find a line ''TIM6_IRQHandler'' there?

Posted on May 17, 2011 at 14:24

Attach the application's HEX file.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sima2
Associate III
Posted on May 17, 2011 at 14:24

Yes, I have checked all your points.

And the application works fine when located at 0x0800 0000.

And I have also move the interrupt vector table using:

NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8100);

It's so stange.

No I have also found when the MCU receives a byte on UART5 I get a Bus Fault exception (a jump to BusFault_Handler().

I have looked at the memory addresses for these interrupt vectors  and they are correct.

I use a STM32F103ZET6 device. Is there any chip errata on this?

sima2
Associate III
Posted on May 17, 2011 at 14:24

Here is the application hex file that I'm experimenting right now to find the problem.

It is located from 0x08008100.

I have scaled away all other code. It only does the following:

int main(void)

{

    TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;

    NVIC_InitTypeDef NVIC_InitStructure;

    NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x8100);

    // System clocks configuration

    SystemInit();

   

    // Enable clocks

    //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);

    //RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA2, ENABLE);

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR |

                           RCC_APB1Periph_BKP |

                           //RCC_APB1Periph_SPI2 |

                           //RCC_APB1Periph_SPI3 |

                           //RCC_APB1Periph_CAN1 |

                           //RCC_APB1Periph_USART2 |

                           //RCC_APB1Periph_USART3 |

                           //RCC_APB1Periph_UART4 |

                           //RCC_APB1Periph_UART5 |

                           //RCC_APB1Periph_TIM2 |   

                           //RCC_APB1Periph_TIM3 |   

                           //RCC_APB1Periph_TIM4 |   

                           //RCC_APB1Periph_TIM5 |   

                           RCC_APB1Periph_TIM6    

                           //RCC_APB1Periph_TIM7 |   

                           //RCC_APB1Periph_I2C1   

                           , ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA |

                           RCC_APB2Periph_GPIOB |

                           RCC_APB2Periph_GPIOC |

                           RCC_APB2Periph_GPIOD |

                           RCC_APB2Periph_GPIOE |

                           RCC_APB2Periph_GPIOF |

                           RCC_APB2Periph_GPIOG |

                           //RCC_APB2Periph_USART1 |

                           //RCC_APB2Periph_ADC1 |

                           //RCC_APB2Periph_ADC2 |

                           //RCC_APB2Periph_ADC3 |

                           RCC_APB2Periph_AFIO, ENABLE);

   

    // Enable CAN RX0 interrupt IRQ channel

    NVIC_InitStructure.NVIC_IRQChannel = TIM6_IRQn;

    NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

    NVIC_Init(&NVIC_InitStructure);

    // ========================================================================

    // Configure TIM6

    //

    // Generate a timer interrupt 6 times per period

    // Time base configuration

    TIM_TimeBaseStructure.TIM_Period = 59999; // Period 60000 = 3.3333 ms

    TIM_TimeBaseStructure.TIM_Prescaler = 3;    // Divide 72MHz with 4 = 18MHz

    TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1 ;

    TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

    TIM_TimeBaseInit(TIM6, &TIM_TimeBaseStructure);

 

    // Clear interrupt flags

    TIM6->SR = 0x0000;

   

    // TIM IT enable

    TIM_ITConfig(TIM6, TIM_IT_Update, ENABLE);

   

    // Enable timer

    TIM6->CR1 |= TIM_CR1_CEN;

}

If i disable the last row (not enabling timer 6) it doesn't fail. But as soon as I activate the timer 6 a Usage Fault exception occurs.

Nickname12657_O
Associate III
Posted on May 17, 2011 at 14:24

Dear SirM,

Your trouble are due to the fact that your application start boundary is not multiple of 0x200 : ''0x08008100''. Please move it to be at

''0x08008200''.

Have a look on our

http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/PROGRAMMING_MANUAL/CD00228pdf

: Page 133 :

''you must align the offset to the number of exception entries in the vector table.

The minimum alignment is 128 words'' , word is 32-bits that means 128 x 4 = 512 Bytes .

This is mainly due to the Vector table size of our High-density devices

0690X0000060MlZQAU.gif

Cheers,

STOne- Your STM32 Moderator.

Posted on May 17, 2011 at 14:24

Your TIM6 interrupt doesn't seem to do much, just increment a RAM variable and leave. It does not appear to actually clear any interrupt, so it will get stuck there endlessly as it repeatedly tail-chains.

Be aware also that SystemInit() is already called before it executes main()

08008354    SUB16    TIM6_IRQHandler:

08008354 B480            push    {r7}

08008356 AF00            add    r7, sp, #0

08008358 F240 0300        movw    r3, #0    ; $0

0800835C F2C2 0300        movt    r3, #8192    ; $2000

08008360 681B            ldr    r3, [r3, #0]

08008362 F103 0201        add.w    r2, r3, #1    ; $1

08008366 F240 0300        movw    r3, #0    ; $0

0800836A F2C2 0300        movt    r3, #8192    ; $2000

0800836E 601A            str    r2, [r3, #0]

08008370 46BD            mov    sp, r7

08008372 BC80            pop    {r7}

08008374 4770            bx    lr

Translates roughly to :

int foo;

void TIM6_IRQHandler(void)

{

    foo++;

}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sima2
Associate III
Posted on May 17, 2011 at 14:24

Thank you very much. I will try that tomorrow.

I have not used high density STM32's until now so I was unaware of that.

Learning all the time.

sima2
Associate III
Posted on May 17, 2011 at 14:24

In the real application I do in fact have a:

TIM6->SR = 0x0000;

, at the entry of the interrupt handler.

I managed to scale away too much when I posted my test code. ;)

And the counter was just to see if the interrupt handler had activated.

sima2
Associate III
Posted on May 17, 2011 at 14:24

When I look at the function header for the NVIC_SetVectorTable() function in misc.c in ST Libraries it says:

@param  Offset: Vector Table base offset field. This value must be a multiple of

0x100

.

There should be some note about this pitfall here?