2015-07-24 2:57 AM
I have been playing around with the STM32F407 for a few days now, learning to set up different timer types and connecting them to each other.
However, most of the examples regard starting timers from external input.My problem regards real-time hardware control at non-periodic points of time, so I need to be able to say that ''time is now A, at time B (B > A) I want timer 1 to generate an event'', which will then fire off a set of sequenced one pulse mode timers and then generate an interrupt at the end of the last timer. I can get everything to work except this:I need that timer 1 to fire off once and then stop. I can probably do this by stopping it in its own interrupt handler, but that seems primitive. Otherwise I could set up timer 1 as a one pulse mode as well but I do not understand how to trigger a timer from software.So in summary: How to I trigger a timer from software?An alternate option is to set up a timer to trigger at a certain point in system time, without software (or interrupt) interference at the trigger time. How would I go about doing that? #trigger #stm32f4 #timer