Triggered Arbitrary PWM with DMA, how to?
NUCLEO-H723ZG
I would like to have a triggered Arbitrary waveform from a Timer.
A defined pattern should be generated, after a Trigger from another Timer.
The arbitrary pattern works well by DMA, but i cannot trigger it.
It's also possible to let it run continously when i disable One Pulse Mode.
But with One Pulse Mode ON, the DMA Update is issued after the next Timer Trigger and not after the last Pulses!
I have DMA Update at TIM_DMA_UPDATE. But TIM_DMA_UPDATE is trigegred when the master Trigger rises. So the DMA is incremented after each Master Trigger.
All samples i found are contiously running..
I dream of a smart Solution with timer settings. Any Ideas/suggestions?
Tnx