Transfer error on SAI4 DMA STM32H723ZE
Hi There,
I'm looking for help with the SAI4 for this device. I have setup the DMA for SAI4A which is linked to BDMA Channel 2. I have defined my buffers within the D3 domain and have enabled the event on the BDMA channel to request number 15 (sai4_a from the reference manual) I still get a transfer error upon starting the DMA transfer. I have watched the training videos on BDMA,DMA and the DMAMUX, but I still think I am missing a step.
I am also having a similar issue on the TIM23_CH2 using DMA but I think if I can find my error on the SAI4 it will be a similar solution for the Timer.
Kind regards,
Kline