cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer Data Program via SPI to FPGA

arduo
Senior

Hi there,

i want to implement my MCU to program a FPGA via SPI. Is there any helpful guidelines on this topic? I am a newbie with STM and i hope that someone can help me here.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

The FPGA documentation should describe the expectations that device has.

The STM32 might need to drive a couple of GPIO, but I'd expect you'd just need to pump a byte or word based bitstream into the SPI Data Register.

Some example SPI code here

STM32Cube_FW_F4_V1.23.0\Drivers\BSP\STM32F4xx_Nucleo_144\stm32f4xx_nucleo_144.c

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..