2020-11-10 8:59 AM
Wondering what are example cases where low-power STM models should be preferred, and what would be the trafe-off in terms of features and performance.
To help me better understand by using specific case, would be happy if I could get 2-3 examples, clear and concrete, demonstrating how a low-power STM vs a standard STM were compared i.e., removing a feature, making a performance decision per a specific case, etc.
Thanks!
2020-11-10 10:19 AM
Seriously? You've never seen a battery-powered device that should last for a certain time?
-- pa
2020-11-10 10:33 AM
Some trade-off:
Low power => low frequencies. In ST datasheet the consumption is uA / MHz!
Low power => use much more software to use sleep modes, switch core/peripheral frequencies, use backup SRAM, configure unused GPIO, etc
Low energy requires special skills.
2020-11-10 1:03 PM
thanks. the "low frequencies" hinted to more search and found this discussion: https://www.researchgate.net/post/What-are-the-pros-and-cons-of-running-a-microcontroller-at-low-and-high-frequency
could you please clarify more about the backup SRAM? is there any impact related memory e.g., Flash?
2020-11-11 4:27 AM
About backup memory:
When the MCU goes to deep sleep (aka standby), the memory (SRAM, FLASH) is unpowered and the SRAM content is lost.
But the application can put some data in a small low power SRAM powered by the VBAT pin : the backup SRAM. So on wakeup the application can recover its context.
2020-11-12 8:59 AM
Thanks Nikita. Very clear and helpful.