2018-06-04 12:55 AM
Hello dear STCommunities,
i am a hardware developper from Germany and i haven't so much experience in TSC (Touch Sensing Controller). In my project i have configure my touch unit in one Group ( 3 pins for my touch electrods and the last one for my sample capacity). My question is do i need to configure a shield imperativly ? i don't have understand exactly his purpose ..
i need help please , an answer will be nice.
Thanks
Eric
2018-06-04 4:32 AM
Take a look at
ST Application Note AN4312. I have done a simple touch sensor without a driven shield, making use of a simple 'grounded shield' as they call it in the Application Note.