cancel
Showing results for 
Search instead for 
Did you mean: 

TIMER

DYann.1
Senior II

Hello,

I found an example on the internet of a project but I don't understand the usefulness of using a Timer 7. Could you tell me why ? Thanks in advance.

 

__IO uint32_t usTick; void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* Prevent unused argument(s) compilation warning */ if(htim==&htim7){ usTick++; } /* NOTE : This function Should not be modified, when the callback is needed, the __HAL_TIM_PeriodElapsedCallback could be implemented in the user file */ } void delay_us(__IO uint32_t Delay){ uint32_t t=usTick; uint32_t wait = Delay; while( usTick - t < wait); } int main(void) { /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM7_Init(); /*if (HAL_TIM_Base_Start(&htim7) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }*/ if (HAL_TIM_Base_Start_IT(&htim7) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } MX_I2C1_Init(); MX_I2S2_Init(); HAL_Delay(100); audio.init(); bool ptt=HAL_GPIO_ReadPin(GPIOE,PTT_SWITCH); bool pttstate=ptt; uint16_t index = 0; uint16_t buf = 0; audio.set_volume(0); /* Infinite loop */ while (1)// read power switch { ptt=HAL_GPIO_ReadPin(GPIO_PINS,PTT_SWITCH); if(ptt!=pttstate){ if(ptt==0){ audio.start_receive(); for(buf=0;buf<32;buf++){ for(index=0;index < AUDIO_BUF_SIZE;index++){ HAL_I2SEx_TransmitReceive(&hi2s2, &i2s_zero,&i2s_buf[buf][index], 1,0xFF); } } audio.start_play(); for(buf=0;buf<32;buf++){ for(index=0;index < AUDIO_BUF_SIZE;index++){ HAL_I2SEx_TransmitReceive(&hi2s2, &i2s_buf[buf][index],&i2s_zero, 1,0xFF); } } } pttstate=ptt; } } }
View more

 

 

40 REPLIES 40

Hi,

Thank you for your helps, I'm guessing but I understand your testing method for the SAI better. Have a nice day.