cancel
Showing results for 
Search instead for 
Did you mean: 

TIMER

DYann.1
Senior II

Hello,

I found an example on the internet of a project but I don't understand the usefulness of using a Timer 7. Could you tell me why ? Thanks in advance.

 

__IO uint32_t usTick; void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* Prevent unused argument(s) compilation warning */ if(htim==&htim7){ usTick++; } /* NOTE : This function Should not be modified, when the callback is needed, the __HAL_TIM_PeriodElapsedCallback could be implemented in the user file */ } void delay_us(__IO uint32_t Delay){ uint32_t t=usTick; uint32_t wait = Delay; while( usTick - t < wait); } int main(void) { /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_TIM7_Init(); /*if (HAL_TIM_Base_Start(&htim7) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }*/ if (HAL_TIM_Base_Start_IT(&htim7) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } MX_I2C1_Init(); MX_I2S2_Init(); HAL_Delay(100); audio.init(); bool ptt=HAL_GPIO_ReadPin(GPIOE,PTT_SWITCH); bool pttstate=ptt; uint16_t index = 0; uint16_t buf = 0; audio.set_volume(0); /* Infinite loop */ while (1)// read power switch { ptt=HAL_GPIO_ReadPin(GPIO_PINS,PTT_SWITCH); if(ptt!=pttstate){ if(ptt==0){ audio.start_receive(); for(buf=0;buf<32;buf++){ for(index=0;index < AUDIO_BUF_SIZE;index++){ HAL_I2SEx_TransmitReceive(&hi2s2, &i2s_zero,&i2s_buf[buf][index], 1,0xFF); } } audio.start_play(); for(buf=0;buf<32;buf++){ for(index=0;index < AUDIO_BUF_SIZE;index++){ HAL_I2SEx_TransmitReceive(&hi2s2, &i2s_buf[buf][index],&i2s_zero, 1,0xFF); } } } pttstate=ptt; } } }
View more

 

 

40 REPLIES 40
DYann.1
Senior II

It's probably to do a clocking in µs ?

Yes, exactly this.

DYann.1
Senior II

Yes but only use in the HAL_TIM_PeriodElapsedCallback and nothing else (the usTick) and apparently the timer works by itself and we don't use it manually to recover the data. I don't see the use of the Timer yet the author says : 'This function Should not be modified, when the callback is needed, the __HAL_TIM_PeriodElapsedCallback could be implemented in the user file'

But there is no callback so why the Timer is necessary ? Thank you for your helps.

TDK
Super User

If the random code you found needs to interrupt at 1 MHz, I would say maybe find a different code to go from.

If you feel a post has answered your question, please click "Accept as Solution".
Pavel A.
Super User

>This function Should not be modified

This looks like just copy/paste from some place in the template code; the HAL_TIM_PeriodElapsedCallback is defined there with "weak" attribute.  In your code it is exactly the "implementation in user file". This function *is* the callback from timer interrupt handler.

/* Example why bad comments are worse than no comments */

 

In this case, I don't need to implement a Timer I guess since there is no callback.

DYann.1
Senior II

Hi, 

I tried to adapt the code to my microprocessor but I don't know which one to choose? In your opinion ?

DYann1_0-1698682177704.png

After me the SAI (equivalent to I2S) work with 3 possible modes: IRQ, DMA and IT. Probably, I'll start with IRQ to make it as simple as possible.

I do this but I get a warning. Do you know how to call the SAI function to retrieve the values ?

DYann1_1-1698683324614.png

Pavel A.
Super User

Source of the ST library is available. Please read the documentation in the library files (.h and c) , it is helpful. The compiler warnings are very helpful - please read them and try to understand the reason.

 

DYann.1
Senior II

Hi,

Just to need the type and now It's correct.

uint8_t txData[16] = { 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 }; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ start_receive (); for(buf=0;buf<32;buf++){ for(index=0;index < AUDIO_BUF_SIZE;index++){ HAL_SAI_Transmit(&hsai_BlockB1,txData,1, 0xFF); } }

But in the example found on the internet the person uses the TransmitRrecieve command. 

HAL_I2SEx_TransmitReceive(&hi2s2, &i2s_zero,&i2s_buf[buf][index], 1,0xFF);

Where to find in the documentation to find the right command to retrieve the values ?