cancel
Showing results for 
Search instead for 
Did you mean: 

Timer controlled GPDMA write to GPIO

SamMiddleton
Associate III

Hi.

In AN5593, How to use the GPDMA for STM32 MCUs, on page 31, it says:

"For some application needs, a timer request to GPDMA can be used to initiate a data transfer not involving timer
registers read/write, but other memory-mapped location, like for memory‑to‑memory transfers."

How exactly do I do this?

My precise use case: I have an 8*3 LED matrix, with the 8 rows connected to PA0:7. I have a uint8_t[3] of the data I want displayed and TIM8 configured at the frequency I want to update the columns at.

Thanks for the help!

1 ACCEPTED SOLUTION

Accepted Solutions
SamMiddleton
Associate III

I figured out a way that works: GPDMA in circular mode (nb: on the u5 series this requires using the linked list mode) with a software request and a trigger on TIM15 TRGO

View solution in original post

1 REPLY 1
SamMiddleton
Associate III

I figured out a way that works: GPDMA in circular mode (nb: on the u5 series this requires using the linked list mode) with a software request and a trigger on TIM15 TRGO