timer capture compare
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-24 6:22 AM
Im going to capture simultaneously 4 input signals(same inputs for 4 channels) using Timer 8 by enabling all the interrupts in TIM->CCER register .. But it was not capturing correctly and im getting channel number 2 and 4 continuously compared to 1 and 3 channels while im giving same frequency for all the channels..
please help me to solve this problem..- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-28 10:42 PM
Thanks for your support..
Frequency is still fluctuating little if i use that math .. ch4_CAP=TIM3->CCR1; ch4_CAP2=TIM1->CNT; if(ch4_CAP2>=ch4_CAP3) { gl31_captval_CH4=((65535*ch4_CAP2)+ch4_CAP)-((65535*ch4_CAP3)+ch4_CAP1); } else { ch4_CAP3=65535-ch4_CAP3; gl31_captval_CH4=(65535*(ch4_CAP2+ch4_CAP3))+(ch4_CAP-ch4_CAP1); } ch4_CAP1=TIM3->CCR1; ch4_CAP3=TIM1->CNT Can you Help me to do the math for both timers..- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-01 6:25 AM
Im still in problem to capture the accurate frequency of cascaded two timers please help me to overcome this problem ..
ch4_CAP=TIM3->CCR1; ch4_CAP2=TIM1->CNT; if(ch4_CAP2>=ch4_CAP3) { gl31_captval_CH4=((65535*ch4_CAP2)+ch4_CAP)-((65535*ch4_CAP3)+ch4_CAP1); } else { ch4_CAP3=65535-ch4_CAP3; gl31_captval_CH4=(65535*(ch4_CAP2+ch4_CAP3))+(ch4_CAP-ch4_CAP1); } ch4_CAP1=TIM3->CCR1; ch4_CAP3=TIM1->CNT; I tried in so many ways but still the frequency was fluctuating (all channels frequencies are fluctuating at the same time)- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-01 8:13 AM
It's a bit of a mess, some of the logic/math is backward, and count should be 65536. This is compounded by a race condition because the high order counter isn't latched, but incremented by a free running counter.
I would use the timer to get the low order precision, and use a high precision, high rate 32-bit counter to mark time and obtain the high order difference.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-01 2:39 PM
This is a blind implementation, as there's no code framework. Assumes TIM3 is slaved off TIM1, and Period=65535; (N-1)
uint32_t captured[6];
void TIM3_IRQHandler(void)
{
uint32_t timebase;
uint16_t timehigh1, timehigh2, timelow;
do
{
timehigh1 = TIM3->CNT; // High order, 1/65536th rate on slave
timelow = TIM1->CNT; // Low order, high rate, will change by a dozen or so ticks
timehigh2 = TIM3->CNT; // Catch rollover, if it occurred
}
while(timehigh1 != timehigh2); // Overflowed, try over, perhaps 1 additional iteration
timebase = ((uint32_t)timehigh1 <<
16
) | (uint32_t)timelow;
// Then for each channel
if (TIM_GetITStatus(TIM3, TIM_IT_CC1) == SET)
{
uint16_t
ccr
=
TIM3
->CCR1; // note use of local/static with same names to limit typos
static uint16_t ccrlast;
static uint32_t timelast;
uint32_t timedelta, ccrdelta;
/* Clear TIM3 Capture compare interrupt pending bit */
TIM_ClearITPendingBit(TIM3, TIM_IT_CC1);
timedelta = (timebase - timelast) >> 16; // error perhaps a few 100 cycles, but we truncate by 65536, so just rounding noise
timelast = timebase;
ccrdelta = (uint32_t)(ccr - ccrlast); // implicitly & 0xFFFF
ccrlast = ccr;
captured[4] = ccrdelta + (timedelta << 16); // Use an array! inherit channel 4 designation
} // sourcer32@gmail.com
// ..
}
Now there is at least one flaw in this method, if the period of the input signal is close to the 16-bit overflow it might underestimate. One way of addressing this would be to compute a rough delta, and compare that to the fine computation. If the rough estimate was around 60000 cycles more, then you have identified a cycle slip in the high order and would correct the fine computation with a += 655
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
‎2013-07-02 10:00 PM
Thank you clive im trying still.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-09 5:34 AM
I got it. i was not given the frequency for the slave timer .. Now it is cleared.. thank you..

- « Previous
-
- 1
- 2
- Next »