cancel
Showing results for 
Search instead for 
Did you mean: 

There seems to be a difference between the system clock immediately after the firmware update and the system clock after the reset (or after power off->on).

YKim.5
Associate

Hello.

I am using stm32f765 series mcu with iar compiler. A strange thing was caught during development and I left an inquiry.

The problem I'm facing seems to be the difference between the system clock right after the firmware is uploaded and the system clock after a reset or power-up.

For example, if i create an 'cnt' variable in the while statement and do 'cnt++', 100 is output immediately after firmware is uploaded, However, when reset or power is re-applied, 80 is output.

Could this happen? If so, when will it occur?

Below is the code for setting my system clock.

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct = {0};

 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};

 /** Configure LSE Drive Capability

 */

 HAL_PWR_EnableBkUpAccess();

 /** Configure the main internal regulator output voltage

 */

 __HAL_RCC_PWR_CLK_ENABLE();

 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 4;

 RCC_OscInitStruct.PLL.PLLN = 216;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;

 RCC_OscInitStruct.PLL.PLLQ = 2;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

 /** Activate the Over-Drive mode

 */

 if (HAL_PWREx_EnableOverDrive() != HAL_OK)

 {

  Error_Handler();

 }

 /** Initializes the CPU, AHB and APB busses clocks

 */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)

 {

  Error_Handler();

 }

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART1|RCC_PERIPHCLK_USART3;

 PeriphClkInitStruct.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;

 PeriphClkInitStruct.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;

 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)

 {

  Error_Handler();

 }

}

Below is the problem area. There is a difference between the value of the 'pp' variable immediately after firmware upload and after the reset. Immediately after uploading, a value of 2400 or higher is displayed, and immediately after reset, a value of about 1200 is output.

while(1){

    pp++;

    SPI_read_data(&hspi3, 0x0B, SPI3_Rx_data, sizeof(SPI3_Rx_data));

    for(int i=0 ; i<DATA_PAD ; i++){

     Data[i] = (SPI3_Rx_data[2 * i] << 8 | SPI3_Rx_data[2 * i + 1]);

     SPI3_Rx_data[2 * i] = SPI3_Rx_data[(2 * i) + 1] = 0;

    }    

    HAL_ADC_Start_IT(&hadc1);

    while(ADC1_flag == 0);

    HAL_ADC_Stop_IT(&hadc1);

    ADC1_flag = 0;

    HAL_ADC_Start_IT(&hadc2);

    while(ADC2_flag == 0);

    HAL_ADC_Stop_IT(&hadc2);

    printf("%d\r\n",pp);

...

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Might be simpler just to print out the current SYSCLK,/AHB APB1CLK, and APB2CLK values are understood on the processor side.

The System Loader will start if the device is blank, several newer models need a power cycle to clear the "BOOT" latch. Programming doesn't clear this.

A debugger may hide the fact it really starts execution from the 0x1FFF0000 vectors.

The SystemInit() or SystemClock_Config() may not handle non-reset conditions well.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

> There is a difference between the value of the 'pp' variable immediately after firmware upload and after the reset.

Okay, and how is this variable initialized? Seems like the first output should be 1 if it's zero initialized, not 1200 or 2400.

If you feel a post has answered your question, please click "Accept as Solution".