cancel
Showing results for 
Search instead for 
Did you mean: 

the throughput of the FSMC in STM32F4XX

live1223
Associate
Posted on May 14, 2012 at 12:55

In my project we want use STM32F4xx, we wonder to know the throughput(max access speed) of the FSMC in STM32F4XX with the condition of the max working frequency(168MHz) of the CORE.

#throughput-stm32f4xx-fsmc #rtfm
1 REPLY 1
Posted on May 14, 2012 at 15:01

In my project we want use STM32F4xx, we wonder to know the throughput(max access speed) of the FSMC in STM32F4XX with the condition of the max working frequency(168MHz) of the CORE.

 

From the data sheet :

''Maximum FSMC_CLK frequency for synchronous accesses is 60 MHz.''

The speed will be further impacted by the settings/cycles for the bus

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..