cancel
Showing results for 
Search instead for 
Did you mean: 

The serial port connection for stm32f4discovery board

hduffddybz
Associate
Posted on July 09, 2015 at 03:28

Hi!I am new to STM32F4Discovery and FreeRTOS,and recently I run FreeRTOS on STM32F4Discovery board,but I found that it is hard to use serial port since there are too many uart pins on this board,so My questions is that how can I successfully connect the ''usb to ttl'' board to Discovery board(You know that B6/B7,A8/A9 all stands for USART1). In addition, I change the value of ''HSE_VALUE'' to 8000000 since the frequency of external crystal is 8MHz.

1 REPLY 1
Posted on July 09, 2015 at 03:49

PA9/PA10 USART1 is not viable due to a capacitor.

Would suggest USART6 via PC6/PC7

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..