2022-08-29 5:57 AM
I need a clarification regarding the actual ADC code equation for SAM4S family of microcontrollers.
The equation from data sheet is,Does this equation hold good for both single ended and differential inputs ?
Looks like it is considering a differential input as the input values subtracted with 2047 and then the gain error is applied on that.
For the single ended inputs the gain error should be directly applied to the input value
2022-08-29 5:59 AM
SAM4S is from ATMEL/MICROCHIP, not ST
2022-08-29 6:01 AM
Thanks, wrong community