cancel
Showing results for 
Search instead for 
Did you mean: 

The difference between VREF+ and VDDA of STM32F407

捷鄭.1
Associate

Is the following note quoted from the specification of STM32F407 applied to all the time from power-up or just during the period when the analog data is being sampled?

「4. If VREF+ pin is present, it must respect the following condition: VDDA-VREF+ < 1.2 V. �?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @�?� 鄭​, to the community!

the note applies to the entire time when Vref is present and not only when analog data is sampled.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @�?� 鄭​, to the community!

the note applies to the entire time when Vref is present and not only when analog data is sampled.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for your prompt reply.​ Then I will generate Vref and VDDA from the same source.