cancel
Showing results for 
Search instead for 
Did you mean: 

Target not responding at the End Node Configuration of P-NUCLEO-LRWAN2

2001jolly
Associate II

Hello,

I am configuring Nucleo-L073RZ with I-NUCLEO-LRWAN-1 expansion board in STM-Cube-IDE as the End-Node with the AT-Master Example in the en-cube-lrwan library provided by ST. 

(en.i-cube_lrwan->STM32CubeExpansion_LRWAN_V2.1.0->Projects->NUCLEO-L073RZ->Applications->LoRaWAN->LoRaWAN_AT_Master->STM32CubeIDE->I_NUCLEO_LRWAN1)

Problem

When I Debug the code into the board it is halted at the HAL_INIT() function.

Solutions I tried

1. There are no breakpoints on it and just below it there a function call for clock configuration and I have also checked it.

2. Performed full chip erase after performing booting.

3. Checked on debugger configuration as well. (Reset Behaviour-> Connect under Reset)

I am attaching the log file also.

 

1 REPLY 1
STTwo-32
ST Employee

Hello @2001jolly 

Could you add a screenshot of the projzct with all the files on the CubeIDE.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.