SystemCoreClock config FAILS on STM32F411RE Custom PCB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-06-30 9:27 PM
Hello All,
I designed a custom PCB that was supposed to run an STM32F411RET6 off an external 8Mhz cystal oscillator.
This is the first custom PCB I have done for an STM32 chip, so I am never quite sure when I am having hardware versus software errors. I have attached some pictures of my PCB below. You'll notice a few 'bodges':
- One of the VCC and VDD pins were swapped in the schematic, so I cut the traces and jumped the decoupling caps. I had to replace the main MCU entirely because of this mistake.
- The BOOT0 pin was left floating, so I have a jumper wire connecting it to GND.
- The VCAP1 pin was left floating, so I have a jumper wire connecting it to VCC (still no capacitor in place).
In order to eliminate some of the guesswork, I am simply trying to configure the HSI and PLL as my application is not really THAT timing critical, plus I have all the other hardware to proof out still.
For what its worth, here are the components I selected for the HSE:
I can connect to the chip with my StLink-V2 via SWD, and can erase & program it with the St-Link Utility.
I am programming and debugging the chip with a trial license of IAR-EWARM.
I have used one of the pre-written STM32F411 Nucleo cube projects to get an ERM motor 'blinking.' The code is shown below:
/* Includes ------------------------------------------------------------------*/
#include 'main.h'/** @addtogroup STM32F4xx_HAL_Examples
* @{ *//** @addtogroup GPIO_IOToggle
* @{ *//* Private typedef -----------------------------------------------------------*/
/* Private define ------------------------------------------------------------*//* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*/static GPIO_InitTypeDef GPIO_InitStruct;/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);static void Error_Handler(void);/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program * @param None * @retval None */int main(void){ /* STM32F4xx HAL library initialization: - Configure the Flash prefetch, instruction and Data caches - Configure the Systick to generate an interrupt each 1 msec - Set NVIC Group Priority to 4 - Global MSP (MCU Support Package) initialization */ HAL_Init(); /* Configure the system clock to 100 MHz */SystemClock_Config(); /*##-1- Enable GPIOA Clock (to be able to program the configuration registers) */ __HAL_RCC_GPIOC_CLK_ENABLE(); /*##-2- Configure PA05 IO in output push-pull mode to drive external LED ###*/ GPIO_InitStruct.Pin = GPIO_PIN_8; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); /*##-3- Toggle PA05 IO in an infinite loop #################################*/ while (1) { HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_8); /* Insert a 100ms delay */ HAL_Delay(100); }}/**
* @brief System Clock Configuration * The system Clock is configured as follow : * System Clock source = PLL (HSI) * SYSCLK(Hz) = 100000000 * HCLK(Hz) = 100000000 * AHB Prescaler = 1 * APB1 Prescaler = 2 * APB2 Prescaler = 1 * HSI Frequency(Hz) = 16000000 * PLL_M = 16 * PLL_N = 400 * PLL_P = 4 * PLL_Q = 7 * VDD(V) = 3.3 * Main regulator output voltage = Scale2 mode * Flash Latency(WS) = 3 * @param None * @retval None */static void SystemClock_Config(void){ RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_OscInitTypeDef RCC_OscInitStruct;/* Enable Power Control clock */
__HAL_RCC_PWR_CLK_ENABLE(); /* The voltage scaling allows optimizing the power consumption when the device is clocked below the maximum system frequency, to update the voltage scaling value regarding system frequency refer to product datasheet. */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2); /* Enable HSI Oscillator and activate PLL with HSI as source */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = 0x10; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 16; RCC_OscInitStruct.PLL.PLLN = 400; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4; RCC_OscInitStruct.PLL.PLLQ = 7; if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2); RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK) { Error_Handler(); }}/**
* @brief This function is executed in case of error occurrence. * @param None * @retval None */static void Error_Handler(void){ while(1) { }}#ifdef USE_FULL_ASSERT
/** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */void assert_failed(uint8_t* file, uint32_t line){ /* User can add his own implementation to report the file name and line number, ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) *//* Infinite loop */
while (1) { }}#endif/**
* @} *//**
* @} */However, the program often crashes when I call HAL_RCC_ClockConfig() function in my main.cpp file.
If I comment out the SystemClock_Config() the program runs, but the SystemCoreClock defaults to 16Mhz.
It usually seems to fail within the stm32f4xx_hall_rcc.c file when either two of the following functions are called:
/* Update the SystemCoreClock global variable */
SystemCoreClock = HAL_RCC_GetSysClockFreq() >> AHBPrescTable[(RCC->CFGR & RCC_CFGR_HPRE)>> POSITION_VAL(RCC_CFGR_HPRE)];/* Configure the source of time base considering new system clocks settings*/
HAL_InitTick (TICK_INT_PRIORITY);Usually if I pause the CPU after hanging here it appears the CPU is in the HardFault_Handler().
Occasionally the program will manually step its way through the entire configuration, but attaching a watch on the SystemCoreClock still shows it at 16Mhz.
Any ideas as to what I should do?
Sorry for not getting the code tags right. Still working on that. Backticks and [code][/code] doesn't either...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-01 3:37 PM
VCC is what in this case?
The VCAP pin(s) should be 1.25V
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-03 8:47 PM
Turvey.Clive.002
‌ I neglected to put a capacitor on the Vcap pin and that seemed to have been the issue. I used a 2.2 uF tantalum cap with an ESR of 7.5 ohm. Now I can connect to it and it seems to work just fine (still having trouble using the MBed stack due to problems with the HSE though...)I am updating the design right now and I am still confused what the correct capacitor value should be for this pin.
Reading this
on page 8 it says that:Vcap2 is not available on all packages. In that case, a single 100nF decoupling capacitor is connected to Vcap1.
I believe this my case, as the LQFP-64 package I am using does only have 1 vcap pin. However later on the app note on page 9 it says
When the voltage regulator is enabled, Vcap1 and Vcap2 pins must be connected to 2*2.2uF LowESR < 2Ohm ceramic capacitor (or 1*4.7 uF LowESR < 1Ohm capacitor if only Vcap1 is provided on some packages.
Which seems contradictory. My best guess is that the 100nF cap is for a processor that has the internal regulator disabled? However, to the best of my knowledge, this pin is connected to the processors internal bus, and that you basically would never want to disable the regulator in the first place?