2016-11-23 6:02 AM
Hi, I have a question about the using of System Workbench and projects.
When I download a firmware from ST website, usually I put the extracted folder in the System Workbench workspace, then click Import -> Existing Project Into Workspace (copy project into workspace uncheked).
It works well, but I obtain a project with relative path and liked resource, I mean that the structure of the files that I can see from Eclipse is not the real structure of the files of the folder project. I don't like it, and it confuse me.
If I want to obtain a ''normal'' structure, I usually copy/paste manually all file in order to recreate the original structure, then I insert include path and symbol. But it is hard and some time leads to compiling errors.There is a way to do it automatically and safely?
2016-11-29 4:24 AM
Hi carbone.fabio,
You would check thishttp://www.ac6-tools.com/content.php/content_SW4MCU/lang_fr_FR.xphp
for this IDE related request/questions.-Hannial-