2018-08-01 10:08 PM
I don't understand why this would compile and work for one project but not another...
const char Menu[40][32] = {
"\033[91;2mShow Menu\033[93;2m <space>",
"\033[0m ",
"1 Read Flash status"
};
char * ptr = &Menu; <- fails here[Clang IntelliSense] Warning: incompatible pointer types initializing 'char *' with an expression of type 'const char (*)[40][32]' VS_EBrakes3F6 c:\users\nickm\documents\vs2018\ebrakesv3_f6\src\bios.c 1107
2018-08-03 4:40 AM
I see a warning only. so compilation succeeded, I suppose. char * insn't const char *, so a warning is ok here. Perhaps in the other project compiler settings are more permissive with respect to warnings?
2018-08-03 5:17 AM
thanks for looking in,
yes, just a warning,
seems to work now, not sure what fixed it :(
but robust now...
2018-08-03 12:57 PM
Menu is an array of 40 constant C-strings, each with a maximum length of 32 characters.
You have set ptr to the address of Menu - so ptr should be the same type as Menu.
If you wanted to set ptr to point to the first string in Menu, then you should have said ptr = &Menu[0];
Do you elsewhere access Menu[1], ...?
Or to access the next menu-item, do you want to say ptr[1] or ++ptr? Because the C compiler would need to know that the size of the element pointed to by ptr is not 1 (sizeof(char)) but 32 (i.e. sizeof(char[32]) ) In which case ptr should be declared/initialised as const char (*ptr)[32] = &Menu;
There's the const-ness as well as mentioned by roland.sonnenschein
2018-08-03 1:25 PM
I haven't seen this style before:
const char (*ptr)[32]
is that the next ptr++ will point to the next string ? adding 32 byte count