Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs Products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs Products
STM32 MPUs Boards and hardware tools
STM32 MPUs Embedded software and solutions
STM32 MPUs Software development tools
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive and Transportation
Microcontrollers
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
RSonn
Associate II
since
2018-08-03
2023-06-14
User statistics
3
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About RSonn
Options
Report User
User Activity
Posts
Replies
I understood that for FLASH of STM32L05x 1 bit error detection and correction is provided. What happens when more bits are corrupted?
2018-08-03
Re: I am using STM32L432KC Nucleo Board. My Vref is connected to 3.3V but I wish to limit my DAC output from 0 to 1 V. How I can achieve this?
2018-08-03
If VDD - VREF is too constrained, use solution through hardware, a voltage divider. This will retain 12 bit resolution.
Re: syntax is the bane of my work...
2018-08-03
I see a warning only. so compilation succeeded, I suppose. char * insn't const char *, so a warning is ok here. Perhaps in the other project compiler settings are more permissive with respect to warnings?