cancel
Showing results for 
Search instead for 
Did you mean: 

SWO functionality

kadam
Associate II

Hello Team,

 

We are developing a custom board based on the STM32N657 MCU. During pin assignment in the CubeMX tool, PB3 is shown with the JTDO_SWO function. However, the datasheet indicates that the SWO functionality is associated with PB5.

Could you please confirm which pin actually supports the SWO function?

kadam_0-1780568138372.pngkadam_1-1780568192964.png

Thanks

1 REPLY 1
Pavel A.
Super User

If you click on PB5 will you see SWO there? 

PavelA_0-1780572276196.png