2015-09-22 02:51 PM
Hi all,
My problem is quite unusual, and I need some new ideas. I can't make SWD connection working on STM32F303RET6. I'm constantly getting ''Can not connect to target'' message.What could possibly go wrong?
#swd #stm32f303ret62015-09-22 03:42 PM
Well isn't one of those chips a 48 pin LQFP and the other a 64 pin? So assuming the chip that works is on a different board, that works, and it STILL points to an issue on the other board related to the debug connectivity.
Perhaps you can use the USB DFU to put code on the board that DOES use the SWD pins, and confirm you can see them toggle, and that you can make them toggle at different rates and confirm you can see both, and they are on the correct pin headers.2015-09-23 03:40 AM
Good idea!
According to STM32CubeMX, the SWIO is PA13, anf SWCLK is PA14. So I did the following code to send two pulses on PA13 and one on PA14: int main(){ setup(); while(1){ GPIOA->BSRRL=GPIO_BSRR_BS_13; // PA13 ON sleep_ms(1); GPIOA->BRR=GPIO_BRR_BR_13; // PA13 off sleep_ms(1); GPIOA->BSRRL=GPIO_BSRR_BS_13; // PA13 ON sleep_ms(1); GPIOA->BRR=GPIO_BRR_BR_13; // PA13 off sleep_ms(1); GPIOA->BSRRL=GPIO_BSRR_BS_14; // PA14 ON sleep_ms(1); GPIOA->BRR=GPIO_BRR_BR_14; // PA14 off sleep_ms(1); } } The result: it works. I see exactly these signals on SWD connector:2015-09-23 08:16 AM
Now I bought another board with ST-Link debugger, and here are my testing results
Debugger -> stm32f4-discovery nucleo-f401re USB Bootloader (DFU)
STM32F303CCT6
yes
yes
yes
STM32F303RET6
no
no
yes
Looks like SWD just doesn't work in STM32F303RET6. .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 {border-width:0px;border-style:none;border-collapse:collapse;font-family:Tahoma;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 tr.telerik-reTableHeaderRow-1 {margin:10px;padding:10px;color:#3F4D6B;background:#D6E8FF;text-align:left;font-size:10pt;font-style:normal;font-family:Tahoma;text-transform:capitalize;font-weight:bold;border-spacing:10px;line-height:14pt;vertical-align:top;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableHeaderFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableHeaderLastCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableHeaderOddCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableHeaderEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 tr.telerik-reTableOddRow-1 {color:#666666;background-color:#F2F3F4;font-size:10pt;vertical-align:top;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 tr.telerik-reTableEvenRow-1 {color:#666666;background-color:#E7EBF7;font-size:10pt;vertical-align:top;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableLastCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableOddCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 tr.telerik-reTableFooterRow-1 {background-color:#D6E8FF;color:#4A5A80;font-weight:500;font-size:10pt;font-family:Tahoma;line-height:11pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableFooterFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;border-top:solid gray 1.0pt;text-align:left;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableFooterLastCol-1 {padding:0in 5.4pt 0in 5.4pt;border-top:solid gray 1.0pt;text-align:left;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableFooterOddCol-1 {padding:0in 5.4pt 0in 5.4pt;text-align:left;border-top:solid gray 1.0pt;} .ExternalClass864ED2B0A0EA474797625FC903C1B31F .telerik-reTable-1 td.telerik-reTableFooterEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;text-align:left;border-top:solid gray 1.0pt;}2015-09-23 10:06 AM
Well they sell a
http://www.digikey.com/product-detail/en/NUCLEO-F303RE/497-15105-ND/5052640
on it, so I'm not entirely convinced it's a chip level issue. Can a J-Link or U-Link access the device? If you built your board with a F401RE on it does that work? Does your debug interface expose NRST and SWO?2015-09-23 10:41 AM
>Can a J-Link or U-Link access the device?
Will try U-Link. But last time it failed even when ST-Link worked (U-Link's SWD never worked for me, maybe something wrong with the drivers or SWD mode just not compatible with Keil 4). >If you built your board with a F401RE on it does that work? Are you asking to solder F401RE off from Nucleo, and put onto my board? Is it pin compatible with STM32F303RET6? >Does your debug interface expose NRST and SWO? Nope, I use 3 wires (TCK, GND, TMS).2015-09-23 12:37 PM
Can't say I've have issues use SWD connectivity with J-LINK or U-LINK pods, but then again I use standard 10-pin and 20-pin type debug headers, and the devices can attempt to ''connect under reset'' as they can hold the devices in reset, or get them into an initial known state.
I suspect the 64-pin configuration is very close, not looking to do the due diligence on that. And don't have an F303 Nucleo to eye-ball the solder bridge or PCB differences.2015-09-23 03:26 PM
Well, U-LINK actually can see the device:
http://svimik.com/ulinkopt1.png
But now I remembered why I stopped using U-LINK some time ago: it throws errors like a rain.First it was: Cannot load flash programming algorithm
Then it was: Invalid ROM Table After playing with reset options (there are many combinations (ok, actually four, but the right one is like a random)) it finally uploaded the firmware, and it even works(!), but the validation fails: Contents mismatch at: 08000000H (Flash=FFH Required=00H) ! Contents mismatch at: 08000001H (Flash=FFH Required=89H) ! Contents mismatch at: 08000002H (Flash=FFH Required=00H) ! Contents mismatch at: 08000003H (Flash=FFH Required=20H) ! But that's another story (that's U-LINK problems, and I'm not sure this is the right place to complain about that). Anyway, it does upload the firmware.ST-Link U-LINK
STM32F303CCT6
yes
yes
STM32F303RET6
no
yes
.ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 {border-width:0px;border-style:none;border-collapse:collapse;font-family:Tahoma;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 tr.telerik-reTableHeaderRow-1 {margin:10px;padding:10px;color:#3F4D6B;background:#D6E8FF;text-align:left;font-size:10pt;font-style:normal;font-family:Tahoma;text-transform:capitalize;font-weight:bold;border-spacing:10px;line-height:14pt;vertical-align:top;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableHeaderFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableHeaderLastCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableHeaderOddCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableHeaderEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;color:#3a4663;line-height:14pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 tr.telerik-reTableOddRow-1 {color:#666666;background-color:#F2F3F4;font-size:10pt;vertical-align:top;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 tr.telerik-reTableEvenRow-1 {color:#666666;background-color:#E7EBF7;font-size:10pt;vertical-align:top;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableLastCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableOddCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 tr.telerik-reTableFooterRow-1 {background-color:#D6E8FF;color:#4A5A80;font-weight:500;font-size:10pt;font-family:Tahoma;line-height:11pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableFooterFirstCol-1 {padding:0in 5.4pt 0in 5.4pt;border-top:solid gray 1.0pt;text-align:left;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableFooterLastCol-1 {padding:0in 5.4pt 0in 5.4pt;border-top:solid gray 1.0pt;text-align:left;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableFooterOddCol-1 {padding:0in 5.4pt 0in 5.4pt;text-align:left;border-top:solid gray 1.0pt;} .ExternalClass9B0958E9846B43628C4006AF34D10684 .telerik-reTable-1 td.telerik-reTableFooterEvenCol-1 {padding:0in 5.4pt 0in 5.4pt;text-align:left;border-top:solid gray 1.0pt;} This reminds me about the first question: why ST-LINK can't work with STM32F303RET6 while it's totally fine with STM32F303CCT6? >I use standard 10-pin and 20-pin type debug headers Well, we make really small devices. This board was 13x36mm, while BoM count is... 79. Can you imagine 10-pin or 20-pin debug header there? 🙂2015-09-23 06:41 PM
The reset options only have any value if NRST is connected. Otherwise you're likely to get weirdness because it can't use a two wire protocol very effectively to wrestle control of the part from all states.
When you can't get a header, being able to escape the signals via castellations or between the layers can help considerably in the design/debug phase. The entire JTAG complement gets you boundary scan, and between the layers a row/panel. I've seen people put SMT land patterns on the reverse side of a board.You said you had the latest firmware on the ST-LINK, which one is that, because we're not getting droves of people here complaining that the Nucleo F303RE isn't working, and the law of large numbers says we would if there was something inherently wrong with the chip or the firmware. The Nucleo boards are up at something like V2.J24.M11