Storing variable in Flash memory
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-08 1:08 AM
I can store variables in flash memory location successfully but what is happening is updating that variable in main.c file not happening.I'm posted code what i have done below.
Linker script file :
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K
FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 153
MY_VARS (xrw) : ORIGIN = 0x08005000, LENGTH = 1K // storing in flash memory
}
.my_vars :
{
*(.MY_VARS*);
} >MY_VARS
In main.c file :
__attribute__((section(".MY_VARS"),myvars)) uint32_t *value=8;
int main()
{
int a =sum(); //i have a sum function of two numbers and storing in variable 'a'
value =&a; // value should updated to sum but it is not updating
readaddress=(const volatile uint32_t *)0x08005000;// reading flash memory
printf("Read flash address %lu\n",*readaddress);// printing the data which is stored in value ,it is printing everytime 8 but it should print variable data which stored in 'a'.
}
int sum(int a)
{
int a=1, b= 34 ;
a=a+b;
return a;
}
Can anybody help me to figure this out,i hope u understood what im asking.
Thank you
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-17 10:35 PM
You could use a function pointer. The address of the function should be ODD. Confirm it's placement by reviewing the .MAP file
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
2019-02-17 10:50 PM
@Community member can you elaborate the answer ?
My understand is ,to create a fun pointer in the flash and excess from the project-2.
what do you mean by ODD ? why it should be odd.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-17 10:56 PM
Odd as in not even. Thumb instruction addresses are designated as odd due to the way the microcontroller decodes them. ie 0x08004001
Up vote any posts that you find helpful, it shows what's working..

- « Previous
-
- 1
- 2
- Next »