cancel
Showing results for 
Search instead for 
Did you mean: 

STMF746 CAN1 Setup

David  Picazzo
Associate II
Posted on July 10, 2017 at 23:56

Good Afternoon! I need help configuring an STM32F746 nucleo board for use with CAN1.  I am using PCAN view to send CAN messages at 250 kBit/s, and CubeMx to generate the initialization code. I am sort of new to this and I am not sure how i should configure the System Clock or what parameters I should use for the Bit Timings in the CAN 1 Configuration. This is the Bit timing calculator I am using but I am unsure of what clock rate I should use: 

http://www.bittiming.can-wiki.info/

. I am trying to migrate working code from a STM32F207 Board with the following Clock Configuration Settings: 0690X00000607OLQAY.png

Thank you for taking the time to help! 

#stm32f746-nucleo #can1
0 REPLIES 0