cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLE5x flash expansion

frnt
Senior

Hello,

I’m wondering if there is a solution to expand the flash memory of the STM32WLEx. I have noticed that the microcontroller do not the Quad-SPI interface. Is there any other possibility to see the external memory as memory mapped?

Any suggestion is welcome. 

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

You'd likely need to attach a NOR Flash via SPI, and map/page code into RAM to execute.

Or pair with a more capable MCU. There are other L4 parts you could pair with a SX1276

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..