2013-07-01 11:44 PM
Hello
I am using IAR embedded workbench tool and STM32W108XX device for development purpose. When I program it I got error message as No reply received.. Error while initializing interface. Please help me asap.. #clive12013-07-02 5:19 AM
I'm not a user of IAR or W1 parts. This doesn't look to be a message from IAR using SWD/JTAG
2013-07-03 3:43 AM
Could you please give us further details? the example you are runnig ? the RF board you are using ?
2013-07-03 8:23 AM
2013-07-03 8:52 AM
These boards?
http://www.st.com/web/en/catalog/tools/PF251361
Are you should you have the STM32W108 in a flashable mode?2013-07-03 10:29 AM
Yes. This is the board I am working on.I have programmed it number of times before it. But now I am getting such type of error..