2013-11-10 2:45 PM
I have STM32VLDISCOVERY board and it works fine till now.
Suddenly I have no more possibility to connect with target from STM32 ST-LINK utility. Following message appears after click to the button �connect to the target�:Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.There is no option ''Connect Under Reset'' in STM32 ST-LINK utility v 3.1.0 #stm322013-11-10 3:49 PM
If the problem with the board is user code, suggest you strap BOOT(0) High and reboot the device, then erase your code.
2013-11-11 12:13 AM
Thanks clive1, your suggestion works.