cancel
Showing results for 
Search instead for 
Did you mean: 

STM32VL-discovery pinout versus protoboard

jabur
Associate
Posted on November 05, 2010 at 20:07

Hi, Why the pinout of the board is so protoboard unfriendly?

I had to tear apart my protoboard to make it work ok...

take a look at

http://maujabur.blogspot.com/2010/11/stm32-discovery-pinout-fail.html

0690X00000602lZQAQ.jpg

3 REPLIES 3
Andrew Neil
Evangelist III
Posted on November 05, 2010 at 23:39

Yes - it is pretty daft, isn't it?!

If you look carefully at the left of this photo, you can see that I adopted exactly the solution as you:

http://www.facebook.com/!/photo.php?fbid=163183327040308&set=a.1627518604167356107434509281857&pid=406728&id=107434509281857

Here's a close-up:

datac99
Associate
Posted on November 12, 2010 at 07:16

Not what I would call ''protoboard friendly'' for sure... But it wouldn't really be a big deal to lop the P3 pins off since they are not going to be mating anyway.

Just a thought 🙂

Andrew Neil
Evangelist III
Posted on November 12, 2010 at 08:08

Still a pain if you actually wanted to use those pins...

Yes, the easiest ''fix'' for ST (without re-spinning the board) would be to simply not fit those pins.