cancel
Showing results for 
Search instead for 
Did you mean: 

STM32VL Discovery Kit Global Pinouts View

STM32 hobbyist
Associate III
Posted on October 18, 2010 at 21:26

Hi all,

I have created an xls file that summurizes all STM32 discovery kit pinouts. This to simplify the developpement with this kit and to have a quick overview on its I/O. It also helps to choose quickly which GPIOs, Timers, communication peripherals... will be used wihout consulting the datasheet. It also indicates which pins are being used by the kit: push buttons, SW, LEDs etc..

I'm waiting your feedbacks.

M3allem

10 REPLIES 10
donald2
Associate II
Posted on September 15, 2011 at 07:43

Added pin numbers for the 48 pin package.

This is useful for prototyping a design that may eventually use the smaller package.