cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 SPI CRC issue

DFell.1
Associate II

Hello all,

I am currently trying to enable the CRC SPI (CRC-16/CCITT-FALSE) on my project, but I can't make it work. 

You can found bellow the SPI configuration set on CubeMx

DFell1_0-1711022577442.png

Here is the message read back on my logic analyser, in yellow (0x0C52) you'll found the CRC computed by the uC.

DFell1_1-1711022737471.png

However with the configuration set I am expecting to get this value: 0xE1F0

From then I suggest that my CRC SPI configuration was not set properly and from an online CRC calculator (https://crccalc.com/) I have check if I could found a match with an another algorithm, unfortunatly I have made no match.

Does any one have a solution to this issue.

 

Many thanks

 

6 REPLIES 6

What would be far more helpful would be the output code, and the registers, especially the CRC register, as you output each of the bytes.

A quick C coding got me 0x1F1F, so no idea where you pulled any of your numbers or expectations.

An for extra entertainment, I ran it thru crccalc.com

crccalc0011.jpg

#include <windows.h> #include <stdio.h> typedef unsigned char uint8_t; typedef unsigned short uint16_t; uint16_t crc16(uint16_t crc, uint8_t byte) { int i; crc = crc ^ ((uint16_t)byte << 8); for(i=0; i<8; i++) if (crc & 0x8000) crc = (crc << 1) ^ 0x1021; else crc <<= 1; return(crc); } int main(int argc, char **argv) { uint16_t crc = 0xFFFF; crc = crc16(crc, 0x00); crc = crc16(crc, 0x11); printf("%04X\n", crc); return(1); }
View more
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for your response.

First what do you mean by "the output code" ? If you refering to the code error send from the HAL_SPI_TransmitReceive command this one is currently HAL_ERROR with the CRC error code fault.

Concerning the SPI register this is the register before the transmission

DFell1_0-1711033739499.png

and bellow the SPI register right after the transmission

DFell1_1-1711033780470.png

 

 

 

By output code I mean what's transacting with the SPI peripheral hardware. The STM32 CRC for SPI has to be initialized, and then transitioned so it sends the CRC bytes rather than data bytes. It typically has no idea where the data stops and the check bytes start.

On the receive side it typically to just pull the data in and the nature of the CRC is to remainder to zero if a copy of the check bytes is passed thru the CRC, and then you "Zero Check" the CRC bytes after the DATA+CRC bytes have processed. But this too has corollaries, as it depends on shift direction, endianness of the chosen implementation/protocol.

ST's general solution to everything is a poor fit to specific / problem things..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

Initial value of the SPI CRC is 0. I don't have the RM at hand now, but I believe that it says so.

JW

I haven't dug into the U5 that deep, but the OP's screen shot shows "Tx Crc Initialization - All One Pattern"

Going to need to walk the transfer and peripheral state one byte at a time to confirm operation and expectations.

 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

Okay, the 'U5 SPI is yet again more complicated, and the documentation is... well... "ST-style". I faintly recall @Uwe Bonnes writing about it recently. And okay, I see, while there's no way to set an arbitrary initialization value, there's a new TCRCINI bit which allows to set the "all ones" as alternative to "all zeros".

And then there's also this:

waclawekjan_0-1711112168443.png

JW