cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 - SDIO emmc

Surya S
Associate II

Hello,

While using HAL_MMC_WriteBlocks API getting TXUNDERR error, please suggest to resolve this issue. Below is the code for reference.

Mode: 8bit

Clock configuration :

SuryaS_0-1689076038480.png

 

 

void Write_SDMMC1(void) {
uint8_t sample_buffer[512] = { 11, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12,
13, 14, 15, 16, 17, 18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29,
30, 31, 32, 33, 34, 35, 36, 37, 38, 39, 40, 41, 42, 43, 44, 45, 46,
47, 48, 49, 50, 51, 52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63,
64, 65, 66, 67, 68, 69, 70, 71, 72, 73, 74, 75, 76, 77, 78, 79, 80,
81, 82, 83, 84, 85, 86, 87, 88, 89, 90, 91, 92, 93, 94, 95, 96, 97,
98, 99, 100, 101, 101, 103, 104, 105, 106, 107, 108, 109, 110, 111,
112, 113, 114, 115, 116, 117, 118, 119, 120, 121, 122, 123, 124,
125, 126, 127, 128, 129, 130, 131, 132, 133, 134, 135, 136, 137,
138, 139, 140, 141, 142, 143, 144, 145, 146, 147, 148, 149, 150,
151, 152, 153, 154, 155, 156, 157, 158, 159, 160, 161, 162, 163,
164, 165, 166, 167, 168, 169, 170, 171, 172, 173, 174, 175, 176,
177, 178, 179, 180, 181, 182, 183, 184, 185, 186, 187, 188, 189,
190, 191, 192, 193, 194, 195, 196, 197, 198, 199, 200, 201, 202,
203, 204, 205, 206, 207, 208, 209, 210, 211, 212, 213, 214, 215,
216, 217, 218, 219, 220, 221, 222, 223, 224, 225, 226, 227, 228,
229, 230, 231, 232, 233, 234, 235, 236, 237, 238, 239, 240, 241,
242, 243, 244, 245, 246, 247, 248, 249, 250, 251, 252, 253, 254,
255, 11, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15, 16, 17,
18, 19, 20, 21, 22, 23, 24, 25, 26, 27, 28, 29, 30, 31, 32, 33, 34,
35, 36, 37, 38, 39, 40, 41, 42, 43, 44, 45, 46, 47, 48, 49, 50, 51,
52, 53, 54, 55, 56, 57, 58, 59, 60, 61, 62, 63, 64, 65, 66, 67, 68,
69, 70, 71, 72, 73, 74, 75, 76, 77, 78, 79, 80, 81, 82, 83, 84, 85,
86, 87, 88, 89, 90, 91, 92, 93, 94, 95, 96, 97, 98, 99, 100, 101,
101, 103, 104, 105, 106, 107, 108, 109, 110, 111, 112, 113, 114,
115, 116, 117, 118, 119, 120, 121, 122, 123, 124, 125, 126, 127,
128, 129, 130, 131, 132, 133, 134, 135, 136, 137, 138, 139, 140,
141, 142, 143, 144, 145, 146, 147, 148, 149, 150, 151, 152, 153,
154, 155, 156, 157, 158, 159, 160, 161, 162, 163, 164, 165, 166,
167, 168, 169, 170, 171, 172, 173, 174, 175, 176, 177, 178, 179,
180, 181, 182, 183, 184, 185, 186, 187, 188, 189, 190, 191, 192,
193, 194, 195, 196, 197, 198, 199, 200, 201, 202, 203, 204, 205,
206, 207, 208, 209, 210, 211, 212, 213, 214, 215, 216, 217, 218,
219, 220, 221, 222, 223, 224, 225, 226, 227, 228, 229, 230, 231,
232, 233, 234, 235, 236, 237, 238, 239, 240, 241, 242, 243, 244,
245, 246, 247, 248, 249, 250, 251, 252, 253, 254, 255,
 
};
 
// memset(write_buffer, 0x0A, 512 * sizeof(write_buffer[0]));
 
HAL_StatusTypeDef status;
HAL_MMC_CardStateTypeDef CardStatus;
uint32_t block_addr = 0;
uint32_t num_blocks = 1;
 
HAL_StatusTypeDef Cardinfo;
HAL_MMC_CardInfoTypeDef pCardInfo;
HAL_MMC_CardCIDTypeDef cardCID;
hmmc1.Instance = SDMMC1;
pCardInfo.CardType = 0;
pCardInfo.RelCardAdd = 0;
Cardinfo = HAL_MMC_GetCardInfo(&hmmc1, &pCardInfo);
 
/* Get the Card CID */
getCardCID();
CardStatus = HAL_MMC_GetCardState(&hmmc1);
status = HAL_MMC_WriteBlocks(&hmmc1, sample_buffer, block_addr, num_blocks,
100);
if (/*HAL_MMC_WriteBlocks(&hmmc1, write_buffer, block_addr, num_blocks, 1000)*/status
== HAL_OK) {
u_writeOk = 1;
} else {
u_writeOk = 0;
}
}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0