cancel
Showing results for 
Search instead for 
Did you mean: 

SDcard->emmc with STM32F205

岡田伸一
Associate

I am using an SD card in SDIO mode with the STM32F205. I am planning to replace the SD card with an eMMC. If the eMMC has SD card mode, can I replace it without changing the program?

1 ACCEPTED SOLUTION

Accepted Solutions
Saket_Om
ST Employee

Hello @岡田伸一 

If the eMMC supports SD card mode and is configured to boot in that mode, it should respond to SD commands just like an SD card.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

View solution in original post

3 REPLIES 3

The MMC has some slightly different initialization commands, and you have to use EXTCSD to determine the block capacity. 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
FBL
ST Employee

Hi @岡田伸一 

I suggest you this application note Getting started with the STM32H7 MCU SDMMC host controller to learn about SDMMC controller to be used to interface your external memory.  

Second, you need to refer to your eMMC specifications to ensure which protocol it supports an to ensure proper initialization. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Saket_Om
ST Employee

Hello @岡田伸一 

If the eMMC supports SD card mode and is configured to boot in that mode, it should respond to SD commands just like an SD card.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om