cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575 can not be waken up from stop mode by LPTIM1 interrupt.

XGao.2
Associate II

I create new StCubeIDE project base on NUCLEO-U575ZI-Q EVB.

Set LPTIM1 as "Counts internal clock events" mode and enable interrupt, set clock source to "LSE".

Did some simple modification in main.c to verify it:

  1. Add #include "stdio.h"
  2. Overwrite weak function __io_putchar to support printf to terminal.
  3. Overwrite weak function HAL_LPTIM_CompareMatchCallback to monitor LPTIM1 interruption.
  4. Add several sentences in while loop. See below code for detail.

When start to run:

Below debugging messages will be shown on terminal. It seems LPTIM1 stopped and wont

trigger interrupt any more. I also tried same thing on L476 board. There is no problem.

Can somebody help me to find if I missed something please?

Can somebody try same testing sequence, help to verify it please?

-- u5_lptm1_wakeup 11:22:33 Sep 13 2022--

in final loop 0

- - - In HAL_LPTIM_CompareMatchCallback - - -

- - - In HAL_LPTIM_CompareMatchCallback - - -

- - - In HAL_LPTIM_CompareMatchCallback - - -

- - - In HAL_LPTIM_CompareMatchCallback - - -

before enter stop mode

.

.

.

/* Private includes ----------------------------------------------------------*/

/* USER CODE BEGIN Includes */

#include "stdio.h"

/* USER CODE END Includes */

.

.

.

int main(void)

{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* Configure the System Power */

 SystemPower_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_USART1_UART_Init();

 MX_LPTIM1_Init();

 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 printf("-- u5_lptm1_wakeup %s %s--\r\n", __TIME__,__DATE__);

 int i;

 while (1)

 {

 printf("in final loop %d\r\n",i++);

 HAL_LPTIM_TimeOut_Start_IT(&hlptim1, 32767);

 HAL_Delay(8000);

 printf("before enter stop mode\r\n");

 HAL_SuspendTick();

// HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

 HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

//  HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

 SystemClock_Config();

   HAL_ResumeTick();

   printf("wake up and delay\r\n");

 HAL_Delay(8000);

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

.

.

.

/* USER CODE BEGIN 4 */

int __io_putchar (int ch)

{

 (void)HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, 100);

 return ch;

}

void HAL_LPTIM_CompareMatchCallback(LPTIM_HandleTypeDef *hlptim)

{

printf("- - - In HAL_LPTIM_CompareMatchCallback - - -\r\n");

}

/* USER CODE END 4 */

.

.

.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Mohamed Aymen HZAMI
ST Employee

Hello @XGao.2​ and welcome to the community,

Can you please share your IOC file with the modified files(main.c).

Mohamed Aymen

XGao.2
Associate II

Uploaded. Thanks

XGao.2
Associate II
 

Any update please?

Mohamed Aymen HZAMI
ST Employee

Hello @XGao.2​,

I apologize for the late reply, I was out of the office for a few days.

I'm working on this issue. I will get back to you shortly.

Thank you for your patience while we work on this.

Mohamed Aymen

Mohamed Aymen HZAMI
ST Employee

Hello @XGao.2​,

Sorry for delayed answer.

I did run your code on my side and didn't work as expected( the system didn't go to stop mode), what I suggest is to try the LPTIMER example from STM32U5CubeFirmware and compare your configuration with the example configuration to see if there is some missing set up ?

Mohamed Aymen

Thank you for your help. I will do more test base on your suggestion.