cancel
Showing results for 
Search instead for 
Did you mean: 

STM32SnippetsL0 - NO SUCH SOFTWARE RESOURCE!

Posted on June 25, 2014 at 22:55

At: http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1898/PF260788

in 'Get Software' section, when we click 'Download' we get the 'stm32snippetl0.zip' (15.1MB file) which contains inside the CubeL0 INSTEAD of the snippetL0.

#stm32snippetsl0
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on June 26, 2014 at 19:18

Yes, it works now.

Thanks a lot,

Bogdan

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee
Posted on June 26, 2014 at 16:18

in 'Get Software' section, when we click 'Download' we get the 'stm32snippetl0.zip' (15.1MB file) which contains inside the CubeL0 INSTEAD of the snippetL0.

It may be a temporary problem that was fixed later. Now this link contains the STM32L0 snippet package (3.17 MB).

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on June 26, 2014 at 19:18

Yes, it works now.

Thanks a lot,

Bogdan