cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L475 RTC interrupt for every 1s

PBala.2
Associate II

I want to configure the RTC interrupt for every 1s in L475. Since all RTC interrupt are routed through EXTI, is it possible to generate the interrupt periodically without depending on external signal?

Something like second interrupt (SECIE) in STM32F103.

2 REPLIES 2
Mohamed Aymen HZAMI
ST Employee

Hello @PBala.2​,

You can refer to the firmware example "RTC Alarm" under this path :

\STM32Cube\Repository\STM32Cube_FW_L4_V1.17.0\Projects\NUCLEO-L476RG\Examples\RTC

Mohamed Aymen.

Thanks @Mohamed Aymen HZAMI​  Will look into it :)