cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KX and WINCE

LMili.1
Associate II

I have a system with WIN CE v6.0 installed and a custom board with micro STM32L432KX.

I've tried to install driver for FTDI but no succes, at the moment WIN CE doesn't recognize the Virtual COM created from my board, are there proper drivers or procedure that I can try?

L.

7 REPLIES 7
Mike_ST
ST Employee

Hello

Do you have an FTDI chip on your custom board ?

LMili.1
Associate II

No I'm using the direct USB of the micro. The test with FTDI is just to test some solution :D

TDK
Guru

Does Win10 detect it correctly?

If you feel a post has answered your question, please click "Accept as Solution".

Yes, on WIN10 and WIN8 without any problem.

L.

LMili.1
Associate II

Yes, on WIN10 and WIN8 without any problem.

L.

WIN CE 6, from 2009, nobody is supporting that.

Perhaps find a generic CDC/VCP driver, and map your VID/PID so that loads/associates.

Other than that you'd need to create an STM32 side CDC/VCP that emulates something your OS supports.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
LMili.1
Associate II

So as a matter of fact I'm no lucky and I can't use something ready to use...undesrtand