STM32L4: Debug is NOT possible when PCROP is activated
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-05 9:57 PM
Hello,
When I enable PCROP for an area of Flash by Option byte, Debugger does not work.
It seems that Debugger has hanged up.
I use IAR EWARM as IDE.
Is it PCROP's specification that Debug is NOT possible when PCROP is activated ?
I think
Debug work well when PCROP is activated.
But I'm not sure it is correct or not.
Could you tell me it is
PCROP's
specification or not?If it is not
PCROP's
specification,
Can you guess why
Debugger has hanged up when I
enable PCROP?Thanks in advance,
K.Higashi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-05 10:22 PM
Dear
kunihiko_higashi
‌,please check application noteAN4758, section 2.4.5.
Best regards,
Tilen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-08 8:48 PM
Dear Tilen MAJERLE,
Thank you for your reply.
I checked AN4758, but I could not solve the problem yet.
So, let me explain the problem more details.
The following is the problem....
I'm using Nucleo-L476RG and EWARM as IDE.
In order to set PCROP, I execute the program below.
HAL_FLASHEx_OBProgram() // for setting Option byte
HAL_FLASH_OB_Launch() // for executing option byte loading
Then, Break instruction does not work.
It seems that Debugger(EWARM) has hanged up, so I must do forced termination to Debugger.
I don't understand why debugger has hanged up.
Do I need any missing functions to solve the above problem?
Thanks in advance,
K. Higashi