[STM32L4] Bit banding
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-15 1:27 AM
Posted on June 15, 2016 at 10:27
Hi,
I want to use the Bit Banding region of STM32L4 but I do not know how to modify the linker script for the same.I tried to follow the https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FC%20compilers%20and%20bit%20banding&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=459and the ARM Infocenter mentioning the C-Code to access the Bit-Banding region starting at 0x20000000 but since I have not seperated the bit-banding region in linker script, the 0x20000000 location gets over written by the code.Can somebody please help me out for the same ?Also, if we use the Bit-band region e.g. 4 bytes of the SRAM bit-band region which translates to 128 (32*4) bytes of bit aliased region, then do I have to leave 128 bytes of SRAM memory in the linker file ?Below is my linker script:; *************************************************************; *** Scatter-Loading Description File generated by uVision ***; *************************************************************LR_IROM1 0x08000000 0x00100000 { ; load region size_region ER_IROM1 0x08000000 0x00100000 { ; load address = execution address *.o (RESET, +First) *(InRoot$$Sections) .ANY (+RO) } RW_IRAM1 0x20000000 0x00018000 { ; RW data *.o (RESET_ram, +First) .ANY (+RW +ZI) } RW_IRAM2 0x10000000 0x00008000 { .ANY (+RW +ZI) }}Thanks,Sunny #stm32l4 #bit-band
Labels:
- Labels:
-
STM32L4 series
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-16 1:26 PM
Posted on June 16, 2016 at 22:26
sorry, operating somewhat blindly here, just modding earlier examples, tested this
LR_IROM1 0x08000000 0x00100000 { ; load region size_region
ER_IROM1 0x08000000 0x00100000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
}
RW_IRAM1 0x20000004 0x00017FFC { ; RW data advance and shrink
*.o (RESET_ram, +First)
.ANY (+RW +ZI)
}
RW_IRAM2 0x10000000 0x00008000 {
.ANY (+RW +ZI)
*.o (.ccm)
}
RW_SRAM_BB 0x22000000 0x80 { ; RW data 4 * 4 * 8, each byte as 8x 32-bit words
*.o (.srambb)
}
}
unsigned volatile long __attribute__ ((section(''.srambb''))) bitBandVar1; // Holds 0x00000000 or 0xFFFFFFFF ONLY
char buf[256] __attribute__ ((section(''.ccm'')));
Execution Region RW_IRAM2 (Base: 0x10000000, Size: 0x00000500, Max: 0x00008000, ABSOLUTE)
Base Addr Size Type Attr Idx E Section Name Object
0x10000000 0x00000100 Data RW 142 .ccm main.o
...
Execution Region RW_SRAM_BB (Base: 0x22000000, Size: 0x00000004, Max: 0x00000080, ABSOLUTE)
Base Addr Size Type Attr Idx E Section Name Object
0x22000000 0x00000004 Data RW 143 .srambb main.o
...
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-06-22 3:36 AM
Posted on June 22, 2016 at 12:36
Hi Clive,
Sorry for replying late.The linker file that you sent is perfect.Really appreciate it.I have just tested it in main(). I need to write proper code to use it in my project, but I guess it should work fine.Thanks,Sunny
- « Previous
-
- 1
- 2
- Next »