Question
STM32f429I crashes when activating TIM8
Posted on April 20, 2016 at 17:53
Hi,
I am using a STM32F429I discovery board and I would like to use the TIM8 with external clock source to trigger ADC conversions. Unfortunately, when I activate and configure TIM8 in STM32CubeMX my application crashes completely (e.g. other timers do not output anything anymore). If I comment out ''MX_TIM8_Init();'' everything works as expected. If ''MX_TIM8_Init();'' is called, the application seems to crash while sending the SDRAM initialization sequence. What can possibly go wrong? And where can I find more information about a possible crash? I am using Keil uVision as IDE. Basically the application outputs some signals with several timers, reads resulting values using the ADC and displays the results on the display. I have ported the configuration for SDRAM and LCD to STM32CubeMX from the board support package, used in the examples.