2019-02-26 01:04 PM
Reference manual RM0038
5.1.1 Independent A/D and DAC converter supply and reference voltage
On BGA 64-pin and all packages with 100 pins or more
I need a bit of clarification on correct voltage ranges for VDDA and VREF+:
2.4 V ≤ VREF+ = VDDA
Does it mean that VREF+ must be equal to VDDA? For instance I have a VREF 2.5V should VDDA be 2.5V as well or can I use 3.3V for VDDA?
2019-02-26 01:46 PM
It seems so for max speed. VREF+ = VDDA for 16 MHz ADC.
From:
STM32L151xE STM32L152xE Datasheet - production data
6.3.17 12-bit ADC characteristics
Table 54. ADC clock frequency