cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L151 and Flash Loader Demo Tool

mmensch
Associate II
Posted on October 17, 2014 at 15:35

Hi,

I use STM32L151 and program it with the Flash Loader Demonstrator Tool. That works fine. Now I wanted to create a small batch file doing it all on one click but there seems to be one little thing not available in the command line options. That is doing an erase of the nessecary pages only. I read somewhere (I don't remember where it was) that STM32L151 can't do a mass erase of the whole flash, so the -e --all option seems to do nothing on an L151. After programming verify fails and the program does only nonsense.

I can produce an equivalent result using the GUI version when selecting no erase.

What can I do? Any undocumented features or workarounds?

Thanks a lot

Martin

1 REPLY 1
Posted on October 17, 2014 at 17:19

What can I do? Any undocumented features or workarounds?

Doesn't the demo come with source code?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..