cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1 up to 512KB Flash

Amel NASRI
ST Employee
Posted on March 05, 2014 at 16:53

STMicroelectronics

 has extended its 

STM32 L1 series

 of ultra-low-power ARM

Cortex

-M3 32-bit microcontrollers with new 512KB flash devices.

0690X00000602rQQAQ.jpg

Key features of the L1 series include

:
  • High-performance ARM Cortex-M3 32-bit core: up to 33 DMIPS operating at 32MHz;
  • Pin-to-pin and software compatibility with all previous STM32 L1 devices;
  • Run-mode dynamic power consumption 257�A/MHz at 32MHz down to 177�A/MHz @ 4MHz
  • Two ultra-low-power modes: down to 435nA with SRAM retention;
  • True embedded EEPROM;
  • Dual-bank flash allowing fast and fail-safe firmware updates and rollback, thanks to the RWW (Read While-Write) capabilities.

The 

STM32 L1 512KB

 is supported by an STM32 Nucleo extension board with mbed

-enabled

.

STM32L1 Series

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1295

STM32L1

http://www.st.com/web/en/news/n3527

#stm32l1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0