cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L05x Standard Library

elb-lab
Associate II
Posted on November 12, 2014 at 09:50

Hi!

I

necessity to use

the standard libraries

for

microcontroller

STM32L052K8

.

If there is

, where

can I download

?

thanks

#stm32l0
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User
Posted on November 12, 2014 at 10:09

There is none and probably never will be.

https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Java%2FSTM32L053%20Standard%20Peripheral%20Library&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&currentviews=768

My personal recommendation is to avoid any ''library'' for the low-level work. The ''Snippets'' show you how.

JW
elb-lab
Associate II
Posted on November 12, 2014 at 11:21

I have a project being developed with a microcontroller STM32F051K8 CoIDE to be translated for STM32L052K8 . The libraries STM32SnippetsL0 can replace the standard libraries ?

waclawek.jan
Super User
Posted on November 12, 2014 at 11:42

> I have a project being developed with a microcontroller STM32F051K8 CoIDE to be translated for STM32L052K8 .

I understand your problem, but I have no easy solution for it. You'll have to either rewrite your project for ''Cube'' libraries (this is what ST would recommend at this moment), develop a (possibly stripped-down) version of the standard peripheral library for the 'L0 (this is what I'd expect from Clive to recommend ;) ), or to rewrite your project for direct register access, without the ''library'' (this is what I would recommend).

There is also a community-driven initiative out there to write a replacement for the Standard Peripheral Library for STM32, but I don't know its status (and I don't even know its name :| )

> The libraries STM32SnippetsL0 can replace the standard libraries ?

No. Snippets are no libraries, they are examples of how to program STM32 low level without any libraries, just using the definitions provided in the stm32xxxx.h header.

JW

Posted on November 12, 2014 at 19:11

Yeah, perhaps...

I don't have much time or effort invested in the L0, though I did go to the seminar the other week.

I guess you have to decide how much effort it is to port it to the HAL libraries, code a subset of the SPL, or go commando and code a register level solution. Given the trade-offs, I might tend toward the latter. The current trend seems to be to make the abstraction thicker whilst make the the speed/resources smaller.

I see the Cortex-M0 as a bit of a design regression. You need to determine what your design needs, and commit resources at that.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..