cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32L053R8 Power consumption is 5mAmps

srm
Associate II
Posted on June 13, 2016 at 14:36

Hello,

As i am designing a project for low power application. The best microcontroller that i had selected is STM32L053R8 which is cortex m0+. Now after drawing shematics according to my application requirement i found that the current consumption of the controller itself is 5mAmp. I am bit confused to see that the low power controller drawing so much of current. I have no clue to slove this issue . I kindly request you to provide me soultion for this. I here by attach controller part schematics that i had drawn uing eagle. If you require any further information regarding this issue i am happy to provide. If there is any problem with schemtics deisgns suggestions are taken in to consideration. Thanks,

Best Regards,

Sandeep.0690X000006039PQAQ.jpg

#lowpower #stm32 #nucleo
1 REPLY 1
Walid FTITI_O
Senior II
Posted on June 13, 2016 at 15:28

Hi

malladi.sandeep.001

,

I recommend that you refer to the 

http://www.st.com/content/ccc/resource/technical/document/application_note/c9/19/d7/b8/6b/0e/4c/d3/DM00051986.pdf/files/DM00051986.pdf/jcr:content/translations/en.DM00051986.pdf

which guides you to establish your design with the best recommendations. (start by adding capacitors between power supply and device’ Vdds)

-Hannibal-