2015-06-29 09:06 PM
I wrote Option Byte and Enalbled Write Protection all flash page.
I can't program MCU. It say flash is protected.How can I fix this problem ?Thank You.Khoa Tran.2015-06-29 10:12 PM
Hi,
You can try using RFlasher from Raisonance to erase config on your micro.Regards,John2015-06-30 01:17 AM
Thank you John.
But I can't find RFlasher..Can you give me the download link ?Khoa.2015-06-30 01:45 AM
Hello tran.khoa,
You can use thehttp://www.st.com/web/en/catalog/tools/PF258168
software.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-06-30 04:57 AM
Hi,
You may need to sign up and download the trail version. It use to be free. Things might have changed. But Mayla's recommendation should work too. I''m sorry I couldn't be more helpful.Regards,John2015-07-01 05:44 PM
Thank you Mayla and John.
I've tried using ST Utility before I started this thread but I can't fix the problem. I may have done something wrong. I will try again.Khoa.2015-07-01 05:58 PM
Well it's a bit hard to trouble-shoot with the information provided.
What exactly did you do to the part originally. How did you write the option bytes, and what exactly did you write to them?Do the utilities indicate is can read the current state of the option bytes, or the content of the flash array?There are definitely things you can do with the option bytes, protection levels, and OTP.Finally you might try to access the System Loader via the USART, this provides access to a selection of commands that might be able to walk the part out of it's current state. These techniques generally require a review of all the relevant documentation and experimentation.2015-07-02 05:43 PM
Thank you clive1.
I fixed the problem with ST Utility.I've tried using System Loader via USART too but It's not working.Khoa.