STM32L051 PLL limit with HSI
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-10-11 12:00 PM
Posted on October 11, 2016 at 21:00
Using an STM32L051, I am unable to generate a 32MHz system clock from from the PLL using the HSI as the clock source. I can generate up to 24MHz without trouble, but any attempt to generate higher frequencies results in the system locking up.
This code fails: // Select internal 16MHz RC oscillator divided by 4 as clock source RCC->CR |= RCC_CR_HSION | RCC_CR_HSIDIVEN; // Wait for HSI ready while (!(RCC->CR & RCC_CR_HSIRDY)); // Enable PLL with HSI as source RCC->CFGR &= ~RCC_CFGR_PLLSRC_HSE; // set PLL source to HSI RCC->CFGR |= RCC_CFGR_PLLMUL24 | RCC_CFGR_PLLDIV3; RCC->CR |= RCC_CR_PLLON; // Wait for PLL ready while (!(RCC->CR & RCC_CR_PLLRDY)); // Change system clock to PLL RCC->CFGR = (RCC->CFGR & ~RCC_CFGR_SW) | RCC_CFGR_SW_PLL; // Update SystemCoreClock to reflect new speed SystemCoreClockUpdate(); If you change PLLDIV3 to PLLDIV4, it works, but at 24MHz. I have tried a wide range of multipliers and divisors, but the limit always seems to be 24MHz. Is this a known issue? If so, it is not in the errata. #stm32l0-pll
Labels:
- Labels:
-
STM32L0 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-10-11 1:46 PM
Posted on October 11, 2016 at 22:46
I found the answer, leaving it here for anyone else who encounters the same problem:
Flash requires 1 wait state when running above 24MHz, so adding this fixes the problem: FLASH->ACR |= FLASH_ACR_LATENCY;