2017-09-21 4:00 AM
Hello,
I'm trying to wake up from STOP mode using LPTIMer on STM32L
LPTIM is clocked by LSE(32K) used as a simple upcounter, and I'm using both ARR and CMP Interrupts from LPTIM, so corresponding bits are set in LPTIM1->IER and NVIC->ISER.
For the purpose of using it in low-power modes I did the following extra steps:
- set LPTIM1SMEN bit in RCC->APB1SMENR
- set EXTI_IMR_IM29 in EXTI->IMR that should let EXTI29/LPTIM IRQ generate a wakeup from STOP event.
It works fine in various sleep modes unless I go to STOP (SLEEPDEEP bit in SCB->SCR) where I stay stuck.
I looked into STM32Cube examples (LPTIM_Timeout,LPTIM_PWM_LSE) and I did not find a clue.
Strangely enough, functions like HAL_LPTIM_Counter_Start_IT even write in bits that doesn't exist in the reference manual like bit 29 of EXTI->RTSR or FTSR... Of course I gave it a try, but without results.
So am I missing something ?
Best regards,
Laurent
#stm32-stm32l0 #low-power #wake-up-from-stop-mode #lptim2019-02-04 7:46 AM
Did you ever get this working?