2019-08-26 1:31 AM
Hello.I am currently developing with STM32L Discovery.
In preparation for development, I tried to output using the MCO in order to know the exact frequency of the HSI of the evaluation board used.
By operating MCOSEL in the RCC-> CFGR register, MSI and LSI could be known, but HSI and the PLL from which HSI originated were not output for some reason.
How can HSI and PLL MCO output be possible?
Please lend me your help.
2019-10-09 6:23 PM
The RCC register was output as follows:
name value address bytes
RCC_CR 0x3000303 0x40023800 4
RCC_ICSCR 0x66b06e 0x40023804 4
RCC_CFGR 0x188000f 0x40023808 4
RCC_CIR 0x0 0x4002380c 4
RCC_AHBRSTR 0x0 0x40023810 4
RCC_APB2RSTR 0x0 0x40023814 4
RCC_APB1RSTR 0x0 0x40023818 4
RCC_AHBENR 0x8007 0x4002381c 4
RCC_APB2ENR 0x201 0x40023820 4
RCC_APB1ENR 0x90000000 0x40023824 4
RCC_AHBLPENR 0x101903f 0x40023828 4
RCC_APB2LPENR 0x521d 0x4002382c 4
RCC_APB1LPENR 0xb0e64a37 0x40023830 4
RCC_CSR 0x1c000000 0x40023834 4
Please let me know if I can do anything else.
Thank you.